External Synchronization of RealSense™ Depth cameras

This week we are introducing a new Genlock function for all RealSense depth cameras which use global shutter imagers. This currently includes the D435 and D435i stereo depth cameras. Genlock allows one or more video streams to be exactly synchronized in time to an external trigger.

This feature is an improvement over our prior multiple camera configuration capability which allowed one RealSense camera to act as the trigger with other cameras in the configuration being driven to fire by the trigger – that feature had some limitations in that only predefined frame rates could be used, and using a non-RealSense device was almost impossible.

Some places where users will find genlock useful are allowing for unique frequencies such as 24fps for film or animation, or significantly slower frame rates. It also allows the use of a separate RGB camera, for example when creating high quality scene captures, using a separate high resolution RGB camera to drive the RealSense depth cameras with perfect synchronization can lead to better results.

Read the whitepaper here

About RealSense

RealSense™ delivers the Visual Cortex of Physical AI™ through industry-leading depth cameras and vision technology used in autonomous mobile and humanoid robots, access control, industrial automation, healthcare and more. With a mission to deliver world-class perception systems for Physical AI and safely integrate robotics and AI into everyday life, RealSense provides intelligent, secure and reliable vision systems that help machines navigate and interact with the human world. The company is headquartered in Cupertino, California, with operations worldwide.

Media Contact


Emily Roberts


PRforRealSense@bospar.com

More News & Insights

    Contact Sales
    Server Region: North America | Hostname: ip-172-16-1-180 | Visitor Country: US