RealSense » 客户案例 » Directed Machines: Robotic automation for smart agriculture and renewable energy

Directed Machines: Robotic automation for smart agriculture and renewable energy


Download Case Study

The challenge

Most autonomous vehicles designed for smart agriculture and renewable energy navigate use global positioning system (GPS) data. However, GPS navigation is not effective in structured environments, such as orchards and solar farms, where the GPS signals are often occluded and noisy.

The solution

The LCR autonomously navigates using RealSense Depth Camera D455, in conjunction with Raspberry Pi microcontrollers. The robot perceives its surroundings in real time, allowing it to operate with centimeter accuracy in both structured and unstructured environments.

The results

RealSense technology provides more features and more value for a lower price than Directed Machines could obtain from competing depth cameras, allowing the company to reduce costs, increase performance, and bring more value to its customers.

A Better Way to Navigate

Land Care Robots autonomously navigate using the RealSense depth cameras in conjunction with programmable Raspberry Pi 4 RP2040 microcontrollers. There is no need for April tags or QR codes or any other type of localization symbols. The robot perceives its surroundings in real time and navigates accordingly.

Advanced vision technology for precision tasks

The LCR samples the depth image at 15 frames per second. The data is channeled through several layers of heavy filtering to remove artifacts and transform it into data representations that can be efficiently manipulated by the CPU: semantic filtering, 2D filtering, and 1D filtering. Since RealSense technology processes the depth data within the camera, it takes much of the load off the robot’s CPU.

The heart of the solution.

Directed Machines’ sensor suite is anchored by two RealSense Depth Camera D455s, which include an inertial measurement unit (IMU) for refined depth awareness. There are two data streams for each camera: RGB data and depth perception data. In addition to navigation, the RealSense depth cameras equip the Land Care Robots with dynamic obstacle avoidance. A compact form factor makes it easy to unobtrusively mount the cameras on the LCR’s solar panel.


RealSense depth cameras fit perfectly into our low-cost, feature-rich sensor suite. Thanks to careful coordination with the RealSense Depth Camera 455, Land Care Robots are fully autonomous and capable of completing multiple tasks without supervision or user intervention.

—Dan Abramson
Co-founder and COO, Directed Machines

What’s

next?

Learn how RightHand Robotics is using RealSense™ computer vision technology to revolutionize automated warehouse order fulfillment.

Robotics

overview

See how RealSense™ cameras can revolutionize the robotics industry with the latest in depth‑sensing technology.


Server Region: North America | Hostname: ip-172-16-1-22 | Visitor Country: US